AXIS#.BODE.PRBDEPTH

Description

AXIS#.BODE.PRBDEPTH sets the length of the PRB signal before it repeats. This applies only when AXIS#.BODE.MODE = PRB. The PRB excitation will repeat after (2^AXIS#.BODE.PRBDEPTH) / AXIS#.BODE.EXCITEGAP drive samples.

Example

Set AXIS1.BODE.PRBDEPTH to 19:

--> AXIS1.BODE.PRBDEPTH 19

Get AXIS1.BODE.PRBDEPTH (already set to 19):

--> AXIS1.BODE.PRBDEPTH 19

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

NA

Range

4 to 19

Default Value

19
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
AXIS1.BODE.PRBDEPTH

5001h

02h

Unsigned8

-

-

Read/Write

No

AXIS2.BODE.PRBDEPTH

5101h

02h

Unsigned8

-

-

Read/Write

No